--------------------------------------------------------------------- SNMPc Integration Kit v1.750 README --------------------------------------------------------------------- DESCRIPTION: This document describes the SNMPc Integration Kit v1.750 operational procedure. ===================================================================== INSTRUCTIONS: (1) Close all active instances of the SNMPc application and/or service. (2) Activate the SNMPcIK.exe file and follow its instructions: (a) Click Next to start the procedure. (b) Click Next to begin backing up the files which will be modified. (c) Click Next to start copying the new files and perform the complete integration procedure. (d) Click Finish to complete the process. (2) After the integration has completed, activate the SNMPc and wait until the MIB compilation has completed. NOTE: If any active instances of the SNMPc application and/or service are running during the activation of the SNMPc Integration Kit, the compilation of the MIB files must be done manually upon completion of the integration procedure.