Our Level-2 shops specialize in providing corrective maintenance for aeroderivative gas turbines, but with one distinction: We keep our repairs local for more convenient and faster service.
There are nine GE Vernova L-2 shops that service the Americas, APAC, and EMEA regions, all with standardized work scopes and capabilities to help ensure consistency.
Level-2 maintenance can be performed horizontally, both for installed and non-installed engines. This includes module exchanges and vane and blade replacement on rotating compressor blades.
All our shop work is conducted under consistent, controlled conditions to make sure that factors like temperature, humidity, and airflow have minimal impact on equipment, procedures and outcomes.
Our shops focus on rapid repair and return of your LM aero fleet. Explore our robust repair capabilities below:
Fleet improvement and local repairs: Improvement and local repairs for your entire fleet, site or unit.
Guidance and support: We help you understand what services are the right fit for you.
Conduct risk assessments: We can help you review the data and evaluate how you can continue running through a detailed engineering risk assessment.
Frequently asked questions
Level-2 maintenance is conducted in the horizontal position either on-site or in our L2 facilities on the external to the package. This includes sensors, actuators, and thermocouples.
The scope of L2 repairs also includes corrective maintenance like modular exchanges, top cases, and hot sections. While many L2 scopes can be done onsite, the advantage of an L2 shop is that it is a maintenance facility with a controlled environment conducive to safe working conditions. High volume shops have dedicated shop leaders and OEM qualified tooling; in many cases, it is within easier reach of our local technicians and typically faster than our L4 shops.
Conversely, our L4 facilities are typically reserved for complete teardowns and major overhauls as well as component repairs.
Repair durations are entirely dependent on scope. Typical timelines for L2 repairs range from a few days to a couple weeks, but each case varies. At GE Vernova, we determine the appropriate shop for your equipment based on repair needs. L4 scopes are usually more complex, leading to longer repair times.
It is our ambition to undertake more scope in our L2 facilities, thereby adding more value to the maintenance chain. However, our capabilities in doing so vary across locations. The U.S., for example, has an installed base that is five times that of Asia. Our team considers that it would be possible to upgrade our Asia shops and match up to 80% of the US shops’ capabilities to meet customer demand.
A site’s ability to operate in a similar capacity as an L2 shop is entirely dependent on its capabilities and facilities. As an example, if a site has an overhead crane with an enclosed climate-controlled space, there's more repairs that can be done locally compared that to a site with none of those types of facilities.
The L2 shops typically take between four and 12 days on average, depending on the work scope and how many work scopes. For example, we can perform a standard hot section repair in as little as four to six days depending on the engine model. If there are additional scopes, then turnaround time increases.
Given the various environments and operating profiles, performance degradation analysis is a unit and site-specific calculation. Upon request, GE Vernova can perform the analysis to assist the customer in determining their specific aggregation over time. If there's an interest in performing an analysis, contact your CSL.
The Level-2 shops follow the O&M manual, and our technicians are trained and qualified to these standards. All our evaluation and services are approved and authorized from our services engineering group.
*Trademark of GE Vernova and/or its affiliates.
Contact us