Proven performance

Our turbine legacy

From higher efficiency and lower costs to faster, cleaner, higher quality power generation, aeroderivative gas turbines have many advantages.

lm2500xpress-R.jpg

The aero advantage

50 years and counting

GE has been in the aeroderivatives business for 50 years, with more than 150 million operating hours and more than 3,000 units in operation.

Aeroderivative turbines can be installed quickly—in as little as a few weeks—to help alleviate frequent outages, making them especially well-suited for utility and industrial applications.

ODC00026-01_Aeros-vs-Recips_web-graphic

Gas turbines yield higher quality power

Plant availability and fuel flexibility

High availability

Aeroderivative gas turbines have the highest availability of any thermal power technology. An aeroderivative gas turbine can be replaced in a power plant, such as a utility or power plant, within a few days for a major inspection, which translates to 98.6% availability.

Diverse fuel options

With the ability to operate on a wide spectrum of fuels—including natural gas, hydrogen, LPG (propane and butane), isopentane, ethanol, diesel, and Coke Oven gas—aeroderivative gas turbines can allow power customers to switch between fuels to save money, all without stopping, and without a reduction in power. Using diverse fuel sources doesn’t just increase reliability, it also results in significant fuel savings—from $12 million up to $43 million per year—as compared to the fuel costs of a high-speed reciprocating engine.

On-demand webinar

The benefits of aeroderivative gas turbines

As a plant operator, you’re always looking for ways to improve your site, and know that higher efficiency leads to lower costs. But what can you do to achieve this? Aeroderivative gas turbines offer many advantages over a reciprocal engine such as reliability and savings instead of maintenance and downtime.

content-aeroderivative-gas-turbines-grid.jpg

Gas turbines create faster power

Getting power to the grid, wherever it’s needed

Fast installation

Because they are small and modular, aeroderivative engines can be transported, installed and commissioned in as little as 3 months. They can be installed outdoors with minimal foundation requirements, making them an advantageous energy solution for any region that needs fast, clean, reliable power.

Fast response rate

GE’s aeroderivative gas turbines feature a power turbine and high-pressure shaft that work together to respond quickly to grid frequency fluctuations, helping create a more stable and reliable grid.

content-aeroderivative-gas-turbines-infographic3.jpg

Aeroderivatives yield cleaner power

Smaller and more stable

Lower emissions

Equipped with best-in-class combustion systems, aeroderivative gas turbines can offer 15 or 25 ppm NOx without needing SCRs (selective catalytic reduction) or the use of ammonia.

Enabling renewables

Aeroderivative gas turbines allow renewables to operate when needed, saving fuel and maintenance—and maintaining a stable grid to allow the integration of more renewables in the future.

Smaller footprint

Because they have about 22 times more power output per unit than comparable high-speed diesel reciprocating engines, GE’s aeroderivative gas power plants take up less space—a real advantage where real estate is expensive. *

*Comparison based on 3 LM2500s (vs. 100 MW of recips).

Customer stories

  • USA
hero-ca-emergency-power-generators.jpg

Inventive NOx scrubbing reduces emissions for California

After recent wildfires and drought conditions, California remains alert and prepared for energy emergencies. Anticipating a supply shortage if hydropower runs dry, the state’s Department of Water Resources (DWR) acted as procurement agent, commissioning four 30-MW GE TM2500 aeroderivative gas turbines. 

Governor Newsom declared safeguarding the grid as imperative, but so was keeping it deeply green, as California sees massive success in meeting its own incredibly strict emissions rules. Honoring this with ingenuity, GE built in selective catalytic reduction scrubbers (SCRs) to the turbines for a markedly low NOX emission rating of 2.5 PPM (opposed to the average of 15). To date, this tech innovation with SCRs is the first of its kind.

Featured video

Aeroderivative turbines vs. reciprocating engines: see for yourself

Curious to learn more about how aeros compare to reciprocating engines? Check out our video to see them go head-to-head.

Contact us

Want to learn more?