Overview

The new hydrogen-capable, combined cycle plant will support the nation’s transition to lower carbon energy.

The challenge

With increasing demand for reliable, sustainable power, YTL PowerSeraya sought a cutting-edge solution that could support Singapore’s growing electricity needs while advancing its energy security and decarbonization goals.

The solution

GE Vernova’s H-class 9HA.01 gas turbine, part of a consortium project with SEPCOIII and POWERCHINA, will power a 600 MW hydrogen-blended facility. This turbine technology, supported by an advanced DLN2.6e combustion system, can operate on up to 50% hydrogen, with potential for 100% in the future, offering both flexibility and lower emissions.

"

By 2027, we intend to expand our power generation capabilities in Jurong Island, Singapore with one of the most advanced natural gas power technologies that is hydrogen-compatible, to help meet the nation’s growing electricity needs and ensure energy security. Our collaboration with GE Vernova on the 600MW hydrogen-capable CCGT project marks a significant milestone in Singapore’s journey toward a more sustainable energy future.

Mr. John Ng

Group CEO, YTL PowerSeraya

Featured video

GE Vernova is powering Singapore

GE Vernova’s 9HA technology is set to drive a major leap in sustainable power generation at YTL PowerSeraya’s new hydrogen-capable plant in Singapore, supplying up to 600 MW to the grid by 2027.

Contact us

Want to learn more about our 9HA gas turbines?