Breathing new life into an older plant
New LM6000 aeroderivative gas turbines are expected to increase both the Russian plant’s reliability and availability.
Overview
A part of Russia’s “Central Black Earth Region,” Voronezh is home to more than a million residents. The 223MW Voronezh Power Plant—owned by Quadra - Power Generation, one of Russia’s largest territorial generating companies—was commissioned in 1933.
In February 2020, GE Vernova announced that the Voronezh CHPP-1 combined-cycle power plant achieved the start of commercial operation, using four of GE’s SPRINT LM6000 gas turbines.
Outcomes
LM6000 simple cycle efficiency
LM6000 combined-cycle efficiency
LM6000 operating hours
This power plant provides heat and power to more than half of Voronezh city’s residential buildings, as well as industrial and social facilities. It is extremely important that the new combined-cycle power unit of the Voronezh CHPP-1 will allow us to reach new heights in the reliability of the city’s heat supply, increasing electric power output by 50% and improving energy efficiency.
Evgeny Zhadovets
Chief engineer, Quadra – Power Generation
GE’s LM6000 aeroderivative technology provides greater flexibility through its fast-start capability (down to five minutes from cold iron), daily/multiple startups with no impact on the equipment maintenance cost and through its low turndown level. An advanced cooling system allows to extend the turbine’s life cycle. This system lowers the high-pressure compressor inlet temperature, which in turn effectively lowers the compressor discharge temperature. The SPRINT module is also equipped with a DLE combustion system providing fuel flexibility and helping to meet emissions limits.
In addition, as part of the project, GE Vernova supplied a modular, multi-stage static air filter unit equipped with an anti-freeze protection system, which will support reliable operation of gas turbines in Voronezh’s winter conditions.
Related products
Case Studies
Contact us