Overview

InterGen, one of the largest independent power producers in the U.K., has ordered High Efficiency (HE) upgrades for its two GT26 turbines at its plant near London.

The challenge

InterGen’s plant 30 miles east of London along the River Thames generates 800 megawatts (MW) of power each year but is seeking to modernize its two GT26 turbines with performance enhancements.  

The solution

Once the upgrades are installed in 2025, the plant is expected to produce 77 additional megawatts of power, gain added efficiency, and reduce carbon emissions by approximately 67,500 tons because less fuel will be required to produce the same amount of energy.

Outcomes

800 MW

currently generated by
the Coryton plant

877 MW

expected after its turbines
are upgraded

~67,500 tons

reduction in carbon emissions each
year after the upgrade

"

GE’s HE upgrade can help increase the output, efficiency, flexibility, lifespan, and availability of the two GT26 gas turbines installed at Coryton, while reducing fuel consumption and environmental impact. Additionally, these turbines are highly flexible and able to operate on a variety of fuels, including blends of hydrogen and natural gas, to offer InterGen pathways to reduce carbon emissions in the next decade.

Jim Lightfoot

CEO, InterGen

“GE’s HE upgrade can help increase the output, efficiency, flexibility, lifespan, and availability of the two GT26 gas turbines installed at Coryton, while reducing fuel consumption and environmental impact. Additionally, these turbines are highly flexible and able to operate on a variety of fuels, including blends of hydrogen and natural gas, to offer InterGen pathways to reduce carbon emissions in the next decade.”

The result is an increase in power output and efficiency and a reduction in carbon emissions.

877

power output with the upgrade

~66,500

tons of carbon emissions reduced each year

The upgrade combines the best from GE Vernova’s F- and H-Class fleets with additive manufactured parts and innovations in aerodynamics, material science and combustion dynamics.

GE Vernova’s Gas Power business had the solution: The GT26 high efficiency (HE) gas turbine upgrade.

UK power producer InterGen needed to modernize its two GT26 turbines to reduce emissions and increase output and efficiency.

Upgrading GT26 gas turbines in London

InterGen, one of the largest independent power producers in the United Kingdom, has ordered GE Vernova High Efficiency upgrades to help modernize its Coryton Power Plant 30 miles east of London. The 800 megawatt (MW) combined cycle power plant uses two GT26 gas turbines that will be upgraded in 2025.

The upgrade, first introduced in 2019, combines the best from GE’s F- and H-Class fleets with additive manufactured parts and innovations in aerodynamics, material science and combustion dynamics. The result is an increase in power output and efficiency and a reduction in carbon emissions. Once the upgrades are installed, Coryton Power Plant is expected to deliver 77 additional MW of power and reduce its carbon emissions by more than 67,000 tons a year.

This will enable the power company to move toward its energy transition goals and stabilize the power grid while keeping costs down for customers. InterGen CEO Jim Lightfood has said the utility chose the GE Vernova upgrade because of its part load efficiency and fuel-flexible combustion system, which will help in reducing carbon emissions.

Contact us

Want to learn more about the HE upgrade for GT26?