Overview

Adding to an already-green energy mix

The challenge

To offset the intermittency of Coachella Valley’s 700+ MW of wind power, CPV needed a proven gas turbine to support its massive, low-carbon Sentinel Energy Power Plant.

The solution

GE Vernova integrated the best technology for the job. The LMS100 is a proven support for “peaking” remediation, especially with its rapid fast start, high ramp rate, and advanced intercooling features.

Outcomes

Renewable ingenuity and a vision made real with the LMS100

800 MW

total plant output

1st                

natural-gas fired project of its kind

640,000+                    

homes needing power in California Edison

"

With California's San Onofre nuclear plant off-line, and power reserves expected to be tight, it’s more important than ever that the CPV Sentinel Energy Project supports power reliability in our summers. The teams did a fantastic job of working with GE Vernova to complete this project ahead of schedule and on budget.

John Murphy

Senior Vice President of Engineering and Construction for CPV

Southern California is highly populated with renewable energy projects, and CPV is adding to it. Its natural gas-fired power plant is capable of providing dependable power under summer peaking, which can easily see triple-digit temperatures. At 800 MW, CPV constructed the world’s largest facility of its kind.

The Sentinel Energy Project integrates the most modern "peaking" power technology around, and that’s GE’s LMS100 aeroderivative gas turbine. Its rapid start (10 minutes) and ramp rate (greater than 10 MW per minute) support the plant with an output of 100+ MW. It has unmatched hot-day performance due to intercooling, and is capable of running on both gas and liquid fuels.

Eight turbines will provide variable dispatch loads—from 50 MW to 800 MW—and a variety of ancillary services, like spinning- and non-spinning reserve. These help firm the local grid and supplement the copious renewable power sources that surround Riverside County.

With GE Vernova adding to gas-fired power plants, and CPV providing a clear path to commercialize greener projects like this one, California sets the example for a clean energy sector; one that provides for 640,000 homes in Southern California Edison's service territory.

 

Contact us

Want to learn more about the LMS100’s supportive intercooling?