Remote diagnostic services for the win
GE Vernova’s remote diagnostic services (RDS) team quickly diagnosed and recommended a successful resolution to a customer before any damage or other negative impacts could occur.
Overview
The customer heard a loud noise inside their gas turbine unit upon startup but the unit was still able to get to full speed no load (FSNL) and no other issues were observed during ramp up. Despite the lack of additional symptoms, hearing such a noise in the unit was quite concerning, especially as this was the second time it had occurred. The customer decided to reach out to the RDS team.
GE Vernova's RDS team utilized the remote services gateway (RSG) workstation at customer’s site to analyze trend data for the concerning startups. The RDS team noticed that the P2 pressure jumped to 185 psi when the speed ratio valve was commanded to open, as compared to an expected value of around 40 psi. They also noticed similar oscillations at certain points during ramp up to FSNL, indicating that the pressure was constantly trying to stabilize.
Outcomes
to diagnose root cause
to diagnose and address issue
savings on potential trips and repairs
saved in potential forced outages, lost generation/availability
Based on these observations, the RDS team determined that the speed ratio valve was causing the issue. The team first recommended that the customer calibrate the valve, stroke it for proper operation, and replace the servos. However, after performing these actions the P2 pressure was still oscillating, so the RDS team determined there was internal damage on the valve making it unable to properly control the pressure. At this point the RDS team recommended replacing the valve as soon as possible to prevent continued rough starts putting additional stress on the unit and eventually damaging the combustion system. Customer followed RDS team recommendation and the unit returned to normal operation.
Main customer benefits:
Contact us