Overview

California knows its hydropower wanes during dry season and peak demand. Two facilities not only got supplemental power, but also built-in SCR scrubbing for super-low NOx.

The challenge

In light of the havoc that California’s recent wildfires and drought have caused, a call to safeguard the state’s energy grid was made as it approached the season of such high demand.

The solution

With fast installation, modular design, and emission curbing, four GE Vernova TM2500 aeroderivative gas turbines were commissioned as a preventive measure against peak-season drain.

Outcomes

A commitment to greener power, even after disaster

2.5

PPM of NOx, notably low compared to an average of 15

hydrogen-fuel capability of the TM2500

120

total MW from four units

After recent wildfires and drought conditions, California remains alert and prepared for energy emergencies. Anticipating a supply shortage if hydropower runs dry, the state’s Department of Water Resources (DWR) acted as procurement agent, commissioning four 30-MW GE Vernova TM2500 aeroderivative gas turbines. 

Governor Newsom declared safeguarding the grid as imperative, but so was keeping it deeply green, as California sees massive success in meeting its own incredibly strict emissions rules. Honoring this with ingenuity, GE Vernova built in selective catalytic reduction scrubbers (SCRs) to the turbines for a markedly low NOX emission rating of 2.5 PPM (opposed to the average of 15). To date, this tech innovation with SCRs is the first of its kind.

The TM2500 is 75% hydrogen-capable, burning far cleaner than gas. With a proven record as backup power and a ramp-up of just minutes, GE’s TM2500 will lend 120 MW to the grid through DWR, who is acting as the generator. 

Kiewit Power Constructors Co. was chosen to install the four units that will shore up California’s ability to respond to future energy-supply crises. Reinforced by the Roseville and Yuba City power plants, the TM2500 is helping reduce the impact of natural disasters on commercial and residential water supplies, not to mention homes and businesses. 

GE Vernova and DWR have reached high for a greener future—through a project that’s added the sustainability and dependability California’s electricity system needs right now.



Featured product

TM2500 mobile gas turbine

Experience the results of one of the world’s most modular, reliable, and experienced mobile gas turbines.

On-demand webinar

Aeros vs. recips: Simplicity in motion

As a plant operator, you’re always looking for ways to improve your site, and know that higher efficiency leads to lower costs. But what can you do to achieve this? Aeroderivative gas turbines offer many advantages over a reciprocal engine such as reliability and savings instead of maintenance and downtime.

Contact us

 Want to learn more about SCR emissions scrubbing and the TM2500?