Prefer to listen?

Stream our audio version*

00:00:00 / 00:00:00

This audio content was developed with the use of Generative AI.

In the fast-paced world of power generation, planning for the unexpected is crucial. Steam turbine outages—whether planned or unplanned—can significantly impact operations, costs, and reliability.

Planning a steam turbine outage comes with unique challenges, as no two turbines are exactly alike in operation or configuration. Even turbines within the same plant can differ significantly due to years of operational factors and past maintenance decisions. 

In this blog, we’ll share insights on best practices for outage planning, covering key challenges, strategies, and emerging trends to help navigate these complexities effectively. 

The growing challenge of steam turbine outages

Each year, approximately 200 outages occur across the steam turbine fleet, with nearly 50% of them unplanned. These unplanned outages often result in costly downtime and extended repair schedules. On average, unplanned outages lead to an additional 3.5 days of downtime, costing around $150,000 in lost generation and increased repair expenses. 

Several industry trends are making outage planning more complex: 

  • Aging assets: Many combined cycle steam turbines are 20+ years old, reaching their second and third major service intervals.
  • Extreme weather events: Unpredictable weather patterns lead to longer and more intense outage peaks, reducing outage windows.
  • Increased cycling: Plants that were once base-loaded are now required to start multiple times per day, accelerating wear and tear.
  • Workforce changes: As experienced engineers and technicians retire, industry knowledge gaps are emerging.
  • Supply chain dynamics: Lead times remain uncertain and haven't returned to pre-COVID levels.

Key failure points and how to plan for them

Effective outage planning starts with understanding common failure points and ensuring contingencies are in place. Some of the most frequent issues include: 

1. Diaphragm and blade wear

  • Over time, some diaphragms may experience dishing and erosion, requiring major repairs or replacements.
  • Inlet stage diaphragms face the most wear due to exposure to high-temperature steam.
  • Planning for long lead-time parts is crucial to avoid unexpected delays. 

2. Valve and casing failures

  • Many steam turbine valve casings and bolted joints develop cracks over time.
  • Conducting proper pre-outage inspections and ensuring availability of replacement bolts and sealants—as well as the equipment required to replace them—can prevent schedule overruns. 

3. Rotor and steam path damage

  • Foreign object debris (FOD), water induction, and thermal stresses can cause rotor and blade failures.
  • Pre-outage borescope inspections and stocking critical spare parts can mitigate risks. 

4. Supply chain delays

  • Post-pandemic supply chain disruptions have extended lead times for essential parts.
  • Partnering with Original Equipment Manufacturers (OEMs) like GE Vernova for early procurement and shared inventory strategies can help mitigate delays.

Leveraging technology for outage efficiency 

One of the biggest advancements in outage execution is the introduction of Live Outage tools. These digital solutions: 

  • Provide real-time updates on work progress and scope changes.
  • Improve crew coordination, ensuring that teams have the right tools and instructions when needed.
  • Reduce outage durations by up to 20% and improve on-time completion rates by 10% with improved productivity tooling, and by better defining contingency plans and optimizing tasks

Why OEM partnership matters 

Working with an OEM  like GE Vernova provides several advantages: 

  • Fleet-wide data insights to predict failures before they occur.
  • Access to proprietary designs and engineering expertise for effective repairs.
  • Stocked inventory and expedited parts supply for faster turnarounds.
  • Field service specialists with decades of turbine-specific experience.

Final thoughts: Be proactive, not reactive

Effective steam turbine outage planning requires early preparation, contingency planning, and strong partnerships. By leveraging data-driven insights, proactive scheduling, and real-time monitoring, power plant operators can reduce costs, minimize downtime, and enhance unit reliability.

If your facility has an upcoming outage, now is the time to start planning to make sure the outcome aligns with your expectations and requirements for the equipment over the next operation interval. 

Reach out to us to make sure your plant is ready for the unexpected!

steam-services-webinar-speaker-mark-kowalczyk.jpg

Mark Kowalczyk

ST & Gen Repairs, Upgrades and Operations Leader, GE Vernova

  • 36 years designing and servicing rotating machinery globally, with 25 years at GEV
  • Experienced in steam turbine design, retrofits, and sealing technologies
  • Expertise in Outage Planning and Execution, with focus on Repair solutions
steam-services-webinar-speaker-matt-foreman.jpg

Matt Foreman

ST, HRSG and Plant Services Platform Leader

  • 18 years in Power Generation/Aerospace industries
  • Experienced in turbine rotor design, steam turbine retrofits, major repairs and product development

*This voiceover has been generated using artificial intelligence technology. While reasonable efforts have been made to ensure accuracy, this voiceover may contain inaccuracies or mispronunciations. The original written blog post remains the authoritative source.

Contact us 

Want to learn more about steam turbine planning?