"The Net Zero Scenario requires the immediate and accelerated scale-up of DAC, calling for an average of 32 large-scale plants (1 MtCO2/year each) to be built each year between now and 2050."


International Energy Agency’s DAC report, 2022

A closer look

How it works

DAC is a promising method of carbon removal that can capture CO2 directly from the atmosphere, creating an opportunity for major carbon reduction. There are several DAC methods including electrochemical cells, solvent-based chemical processes, and solid sorbent-based chemical processes.

GE Vernova sees sorbent-based chemical processes, which can be categorized as low temperature and/or vacuum swing, high temperature swing, or moisture swing, as one of the more promising forms of DAC. The process is described in more detail below.

DAC value chain

The carbon journey

See below how carbon is captured, processed, and leveraged.

dac-diagram-1920x1080.png
Blue and Black Bar Chart Presentation - Visual Chart Page Iteration 2

A legacy of innovation

Experience matters: 14+ programs demonstrating DAC capabilities

When it comes to developing breakthrough technology, we’ve been working to develop our DAC technology with several organizations, including several U.S. government departments and agencies.

View the five programs we've selected to highlight in the chart on the right.

On-demand webinar

Industry innovators: The technology path to more reliable and sustainable decarbonization

Watch our webinar to learn about self-healing grids, air-cleaning power sources, and AI-enhanced wind turbines. Furthermore, you can discover DAC breakthroughs and grid modernizations for faster power restoration.

Partnering for success

Why choose GE Vernova?

We are among the few companies with all required competencies for scaling DAC under one roof. Our highly experienced research team positions us well to develop effective sorbent materials. Furthermore, our decades of experience with power plants and accessories enables us to provide a state-of-the art system design.

We have what it takes to make DAC a reality in the very near future.

FAQs

Have questions on DAC?

How are CCS and DAC different?

Carbon Capture and Storage (CCS) typically refers to capturing CO2 from point sources (i.e. at the point where CO2 is emitted), whereas Direct Air Capture (DAC) can capture CO2 from ambient air.

DAC is a type of CCS technology, in that it’s a branch of applied science aimed at reducing carbon dioxide (CO2) in the atmosphere. Captured CO2 from DAC or CCS can be stored in geological formations such as depleted oil and gas reservoirs, deep saline formations, or through mineralization processes.

DAC (Direct Air Capture):

  • Captures carbon directly from ambient air, with flexibility in facility location
  • Uniquely suitable for capturing CO2 in hard-to-abate sectors, as well as legacy and future emissions

CCS (Carbon Capture and Storage):

  • Describes a range of technologies that capture CO2 emissions, typically from point sources like power plants, cement factories, and other industries
  • Involves transporting captured CO2 to secure underground storage sites

Why does GE Vernova care about DAC?

As an industry leader who helps generate 30% of the world’s electricity, GE Vernova recognizes our responsibility to not only deliver more sustainable, reliable, and affordable power, but also spearhead global decarbonization initiatives. We’re committed to both environmental stewardship and a more sustainable future.

What government grants and funding are available to help pay for DAC?

United States
The US Inflation Reduction Act (IRA) offers large incentives for direct air capture, including $3.5 billion for regional DAC hub research, development, and demonstration. Additionally, the IRA offers tax credit of $180/tCO2 captured via DAC for storage, with a capture threshold of 1,000 tCO2/year. Further proposed legislation in the US aims to create government procurement programs for the purchase of proven CO2 removal technologies.

European Union:
Horizon Europe offers funding for research and innovation projects across various sectors, including cleaner energy and climate change mitigation. DAC projects may be eligible for funding under relevant Horizon Europe programs, such as the European Green Deal Call.

The EU’s Innovation Fund supports the demonstration of innovative lower carbon technologies, including carbon capture and utilization (CCU) projects. DAC initiatives could potentially receive funding through this mechanism.

Australia:
The Low Emissions Technology Development Fund supports the development and deployment of lower emissions technologies, including carbon capture and storage (CCS) projects. DAC initiatives may be eligible for funding under this program's CCS Stream.

The Australian Renewable Energy Agency (ARENA) offers funding for renewable energy and lower emissions projects, including innovative technologies that contribute to emissions reduction and climate change mitigation.

How can carbon captured during DAC be repurposed if not stored?

  • Fuel Synthesis: Conversion into synthetic fuels like methane or methanol
  • Chemical Production: Use in feedstock for producing chemicals, plastics, and fertilizers
  • Mineralization: Chemical reaction to create stable carbonate minerals for construction materials, like concrete.
  • Enhanced Oil Recovery (EOR): Injection into oil reservoirs to enhance oil recovery
  • Agriculture: Utilization for greenhouse enrichment, carbon fertilization, or algae cultivation

Why is GE Vernova well-positioned to help decarbonize at scale?

Not only do we have the experience, but our current projects collaborating with US government organizations demonstrates that we’re forging the path ahead in this space. With a passion for innovation and a diverse portfolio of leading technologies, we can help reduce the carbon-intensity of the world’s power systems by reducing the CO2 per kWh produced.

Contact us

Want to know more about GE Vernova’s DAC activities?