Prepare your B&E rotors for the future with life management solutions
The history of GE's B- and E-fleets dates back over half a century. As the OEM, GE Vernova knows exactly what's in your gas turbine, right down to rotor versions and replacements.
Plan ahead!
Aging plants, changing operating demands, regulatory uncertainty and increasing cost pressures make it more important than ever to cost-effectively manage and maintain gas turbine rotor assets. We have solutions to help keep your fleet in operation while reducing downtime for the long term.
Benefits
When it comes to rotor life management and extension, GE Vernova has the advantage. With our vast OEM knowledge and experience, we can help repair and extend the life of your rotor and keep it running safely and reliably.
The most experience
Across the gas turbine B- and E-fleets, there have been over 100 rotor end-of-life solutions applied on the welded rotor fleet and more than 160 solutions of the bolted rotor configurations since the 1990s. When it comes to addressing gas turbine rotor needs there are many different solutions, but GE Vernova has the knowledge, history, and expertise to perform a full rotor-life assessment, addressing all phases of the lifecycle—for today and tomorrow.
Through years of fleet and engineering analysis, we have developed proprietary gas turbine rotor manufacturing processes that cannot be duplicated. As rotor assets have aged over the last few years, our customers have worked with us to replace more than 250 B and E turbine rotors and over 500 F turbine rotors. For the 7F gas turbine there have been more than 30 turbine rotor modifications, 10+ compressor rotor enhancements, and more than 100 different blade changes since 1990.
Customer stories
plant life extension
rotor life extensions
Myanmar Lighting owns a 230 MW combined-cycle gas power plant located in Ngan Tae, Mawlamyine that is powered by three 6B gas turbines and one LM2500 gas turbine supplied by GE Vernova that have been in operation since 2014. Knowing that the 6B gas turbine rotor end life was approaching in 2022, the customer needed a long-term solution to ensure that the plant could continue to support the growth and needs of the people of Myanmar. GE Vernova developed a 6B rotor life management solution to help the utility continue supporting Myanmar’s energy sector.
The GEVSS*
Building on 45 years of technology innovation in HA gas turbine components and repair and with the support of the Singapore Economic Development Board, GE Vernova has established the GE Vernova Singapore Services (GEVSS) facility to better service HA power plant operators based in Asia and countries outside the Americas region, supported by BGGTS and GEMTEC. Learn more about repairs and service centers in Asia.
*GEVSS formerly known as GRSS.
Frequently asked questions
Planning for rotor life management begins with the following key questions:
Based on your plant’s long-term strategy and decision-making processes, planning should begin as early as three or more years in advance—when the rotor has approximately 150,000 FFH or 3,500 FFS. Early planning gives you the time and flexibility to examine available solutions and find a good match for your plant’s long-term vision. After the plan is set, GE Vernova works with you to build the right solution.
We have a 3-pronged approach:
Safe operation starts with GER-3620, which provides a general overview of the best operating and maintenance practices for GE’s heavy duty gas turbines. It describes how factors such as time, cycle, and temperature impact the life of the rotor and other gas turbine components. The guidance also explains how to document and track rotor life consumption based on listed maintenance factors and the unit’s fired hours and starts.
Inspections must be employed at normal outage intervals as outlined in GE’s Technical Information Letters (TILs) which have been released over the past years. TIL-1049 describes inspections of the turbine wheel dovetail for material loss while TILs 1805/2056 covers inspection of the 9B/9E compressor stub shafts. To help maintain safe rotor operation until the next inspection interval, the TILs associated with each specific unit should be reviewed and all outlined inspections should be performed during normal outages such as a hot gas path or major inspection outage. Each of these inspections are done during normal outages like a hot gas path, major inspection or C-inspections and will help ensure that the rotor can operate safely to the next inspection interval.
The last step of a robust maintenance and inspection plan involves performing a rotor overhaul to help ensure continued safe turbine operation, when the time is right. Appropriate timing for a required rotor overhaul must be based on operating history and maintenance factors as outlined in (TILs) 1576, 2040, 2197 and GER-3620.
Building the best-fit solution and selecting the rotor life plan that best meets your specific needs requires examining three different options:

Further reading