GE’s OpFlex solution leading to larger profits
In an effort to increase efficiency and productivity, Mainova had GE Vernova install their OpFlex control software technologies on a 6B gas turbine in Frankfurt.
Overview
In Germany, cogeneration using gas fuel is competing in a landscape where electricity sells on a daily basis and purchases are mainly driven by the price of fuel. Other less costly fuel sources, such as solar, wind, coal and nuclear take precedence, leading Mainova to take an innovative step to drive production efficiency.
The GE Vernova unit in Frankfurt was the first 6B gas turbine in the world to receive OpFlex control software technologies: AutoTune, Turndown, Variable Peak and Smart Inlet Bleed Heat (IBH). This Advanced Controls solution is designed to deliver broad operational flexibility across all modes of plant operation by expanding the operating envelope, while enabling significant performance improvement.
Outcomes
turndown to 40% load
emissions compliant peak load
fuel savings during partload operation
Mainova is now able to run their gas turbine at competitive levels, leading to a more profitable position in the market. They also now have the ability to set emissions limits and let the turbine control maximum performance within those limits. One of the biggest benefits Mainova saw was the ability to expand their emissions-compliant operating range from 60–100% load to 40–110% load.
Case Studies
Contact us