Overview

A new Combined Cycle Power Plant (CCPP) began operating to help keep pace with South Korea’s fast evolution, expansion, and call for greater power—along with the ability to lower its carbon output.

The challenge

With a rise in energy demand born from economic growth, in addition to upgrades to its existing facilities, KOSPO needed to construct a new facility for addition generating capacity and future-looking greenhouse emissions control.

The solution

The new Shinsejong CCPP uses GE Vernova's 7HA.03 gas turbine along with the DLN 2.6 combustion system; a combo that bolsters performance and operational flexibility while reducing CO2 and NOx emissions. Shinsejong marks GE Vernova's 100th HA turbine installation.

Outcomes

Transition to a low carbon future

160,000

homes potentially powered by KOSPO’s energy

NOx at the main stack, using DLNe 2.6 combustion

+64%

net combined cycle efficiency of the 7HA.03

"

We are honored to support KOSPO in reducing carbon through power and thermal energy via liquefied natural gas. Natural gas-fired combined cycle power plants are the lowest emitting fossil fuel power plants, and with South Korea’s power generation stemming primarily from fossil sources, the 7HA will play a critical role in the transition to its lower carbon future.

James Kim

GE Vernova, Country Leader, South Korea

South Korea is headed upward. With ranking 1st in the Bloomberg Innovation Index of 60 nations, the highest broadband penetration in the world at 97%, and a projected 4% annual GDP growth, South Korea is poised to bloom as a technology leader. Steadily powering 11% of the country as its largest utility, KOSPO sought state-of-the-art solutions to meet increasing demand while reducing carbon emissions.

“Only those who prepare themselves will meet a prosperous future” is KOSPO’s philosophy; one that well aligns with South Korea’s “Green New Deal”: a transition from fossil fuels, development of a hydrogen economy, and expansion of renewables, all aiming at carbon-neutrality by 2050.

With GE Vernova as partner, a proven H-class evolution was integrated into the new Shinsejong CCPP—the 7HA.03 gas turbine. It's the largest, most efficient turbine in the world, with the lowest cost conversion of gas to electricity in a 60-hertz platform. Its modular configuration also enables greater plant economics and faster installation for engineering, procurement, and construction vendors.

Complementing the turbine is GE Vernova’s DLN 2.6 combustion system with advanced premixing. This adds fuel flexibility and performance, also empowering KOSPO to lower NOx emissions.

GE Vernova's gas turbines provide more than 14,000 MW of generation capacity in South Korea. The new unit is driving the performance of KOSPO’s Shinsejong CCPP, which is the first plant in the region powered by one of GE Vernova's 7HA.03 gas turbines. GE Vernova is proud to help supply grid power, district heating, and air conditioning to Sejong City, the administrative capital of South Korea.

Featured Video

See our first team-up!

GE Vernova and KOSPO have joined forces before. During a key point in South Korea’s growth, GE Vernova’s fleet upgrades to KOSPO’s Shin-Incheon and Busan plants resulted in an additional 215 MW—enough to energize 160,000 homes.

Contact us

Want to learn more about our AGP and DLN solutions?