Transforming grid planning

The power industry is evolving. So should the software you use to understand it.

The PlanOS software platform offers a holistic approach to planning your energy system’s most pressing challenges. With the option to augment your modeling with GE Vernova’s robustly-mapped power system dataset, you can enhance your analysis and accelerate model development.

Your unified dataset model can seamlessly flow between native single- or multi-function analysis – enabling a truly integrated experience.

Integrated planning functions

Revolutionize your system planning experience

PlanOS is powered by the robust algorithms of our decades-proven planning software—MAPS, MARS, and PSLF—to help you break down traditional planning silos.

Analyze the economics, reliability, and power flow of your system, and confidently plan for capacity expansion—all from a single platform. 

PlanOS

Watch to learn more about integrated system planning.

Webinar

PlanOS: Prepare for the energy transition with a fully integrated grid planning platform

July 31, 2024 | 11 am Berlin time, 11 am New York time

Experience end-to-end grid planning with a unified dataset and a native, simplified infrastructure by leveraging the capabilities of the PlanOS modules formerly known as PSLF, MARS, and MAPS. Join our webinar to learn more!

Jim Walsh

General Manager, Consulting Services, GE Vernova

Jason MacDowell

Senior Director, Consulting Services, GE Vernova

Dr. Sheila Manz

Technical Director Decarbonization Planning, Consulting Services, GE Vernova

May Millies

Executive Commercial Leader, Americas, Consulting Services, GE Vernova

Frequently asked questions

Discover the advantages of Integrated Systems Planning

What is Integrated Systems Planning and why is it important?

With the growth of inverter-based resources and the increase in variable loads on the grid, it’s critical for system planners to consider more comprehensive planning approaches to help identify and solve issues holistically. Integrated Systems Planning is an approach to energy planning that considers all aspects of an energy system aiming to improve the system for cost-effectiveness, sustainability, and reliability by coordinating them together, rather than planning each element separately. This holistic approach provides an improved understanding of resources and their performance while aiming to ensure cost-effective reliability. 

Traditionally, the analyses that feed into system planning, like resource adequacy, cost of production, and power flow, are conducted in silos and often rely on different data models, assumptions, and factors. This traditional siloed approach to system planning may result in inaccurate or disassociated insights. 

What is the difference between GridOS and PlanOS?

GridOS enables a unified dataset model for the near or real-time operations of the power grid. PlanOS utilizes your dataset focused on long-term planning analysis.  

As GE Vernova continues to provide solutions that help you stay ahead of grid complexity, both in terms of operations and planning, the thoughtful architecture of our solution is meant to provide the fidelity of unified data that is appropriate for the context of analysis you need. Spend your time where it matters, planning the grid of the future—not connecting disparate data sets and building multiple data models.  

How should current PSLF, MAPS, and/or MARS users think about PlanOS, and what can they expect?

PlanOS is the platform in which your unified dataset model can seamlessly flow between native single and/or multi-functional analyses. Previously known as PSLF, MAPS, and MARS, now known as Power Flow, Production Cost, and Resource Adequacy, PlanOS is built on the industry-proven algorithms you have grown to trust with expanded capabilities and soon a refreshed user interface. With the ability to utilize robust grid models of over 50+ countries developed and maintained by GE Vernova (an industrial and software company–we understand the hardware) you can enable your journey even faster. Contact GE Verona’s Consulting Services to learn about our high-fidelity models.

Is this platform just an updated UI to interface between GE Vernova’s software products, or is it a new program altogether?

PlanOS is not just a new user interface, nor is it a new software program. PlanOS is a platform where your unified dataset model can seamlessly flow between GE Vernova’s native modular applications. It is the foundational architecture to streamline data portability, versioning, and branching at speed. For customers with more than one of GE Vernova’s planning functionalities (Steady State Power Flow, Resource Adequacy, Production Cost, and soon-to-be-released Capacity Expansion), the standardized and enhanced user interface provides a consistent user experience that is modern and intuitive.

How will PlanOS reduce simulation time while meeting all system constraints?

PlanOS enables cross functional analysis with the same data set. The PlanOS architecture aims to ensure simulations run faster without altering the model unless you intend to for accurate results.

PlanOS’ native infrastructure emphasizes accelerated planning analysis and model portability, helping to eliminate the need for manual data file conversion or the recreation of model format files for analysis. 

What are the additional functionalities available with PlanOS?

GE Vernova’s proprietary Contingency Analysis (evaluates the impact of potential issues or unexpected events) and Transfer Analysis (evaluates the maximum amount of power that can be moved without violating system limits) capabilities will be native functionalities available for both power flow and resource adequacy analysis. This simplifies the number of software applications and APIs needed to interface with the software. Unlike other solutions, GE Vernova’s PlanOS also has built-in algorithmic processing and analytical capabilities. This enables faster analysis without relying on third-party algorithmic processing software, simplifying your IT infrastructure for planning analysis, and helps save your business time and money. 

Is PlanOS compatible with other planning software?

PlanOS is enabled with proprietary APIs for file conversion before or after analysis efforts, making it compatible with most industry file formats and planning software. 

How is customer feedback incorporated into product development?

GE Vernova collaborates with our customers, system operators, regulators, policymakers, and developers worldwide to incorporate various regulatory and industry-leading enhancements into the software. 

Additionally, we are our own customer. GE Vernova’s Consulting Services uses PlanOS for our global studies and assessments. We have developed and maintained commercially available models of over 50 countries, adapting to different grid codes, connection standards, and industry mechanisms.

Can PlanOS consider regulations in different countries?

Yes, the functions of PlanOS can comply with different grid codes, connection standards, industry mechanisms, and user requirements. This global approach allows GE Vernova to effectively apply lessons learned from developed regions to developing areas, addressing universal and localized grid challenges.

Contact us

 Want to learn more about our PlanOS capabilities?

*Trademark of GE Vernova and/or its affiliates.