Skip to main content
press release
Gas Power

GE Gas Power and Shell sign Development Agreement to collaborate on LNG Decarbonization Pathway Using Hydrogen

6 min read
  • GE will collaborate with Shell to develop potential lower-carbon solutions aiming to reduce the carbon intensity of Shell’s LNG supply projects around the world
  • Under this agreement, GE will accelerate development for the use of 100% hydrogen as a low carbon fuel for gas turbines
  • Focus will be on hydrogen solutions for B&E class gas turbines used in LNG and power generation applications

Atlanta, GA; November 7, 2022 – GE Gas Power (NYSE: GE) and Shell Global Solutions, a pioneer in liquefied natural gas (LNG) for more than 50 years, announced today they have signed a development agreement to pursue potential pathways aiming to reduce the carbon intensity of Shell’s LNG supply projects around the world. With global LNG demand projected to almost double by 2040, decarbonization is crucial in helping the company meet the world’s growing energy needs.

The largest source of emissions in an LNG facility stems from firing natural gas in the power generation and mechanical drive gas turbines. Therefore, one of the possible paths to decarbonize LNG production is to use hydrogen as a low carbon fuel in these engines. However, the source and nature of this fuel matters as well, and Shell’s Blue Hydrogen Process is a leading technology that can deliver the lowest carbon intensity fuel of its kind, with technologies and building blocks tested and commercially proven at a large scale, that have been used in various industries for many decades.

“Having worked on hydrogen combustion technologies for many years, we are conscious that progress in this area will be the result of careful, dedicated research and collaboration by industry leaders and today’s announcement is a model of this approach,” said John Intile, Vice President, Engineering at GE Gas Power. “We look forward to working in cooperation with Shell to advance this crucial body of work. Together, we’re confident our combined strengths of Shell, GE, and Baker Hughes, who is exclusive distributor of certain heavy duty gas turbines and services in the oil & gas segment, can accelerate the deployment of pragmatic and impactful solutions towards high-hydrogen capabilities in these gas turbines fleets resulting in a significant reduction of carbon emissions and water utilization globally.”

The deep decarbonization of LNG export facilities presents both technical and economic challenges, which need to be addressed to realize such ambition. “Becoming a net-zero emissions energy business means we need to explore a range of avenues that have the potential to help us, our partners and customers reduce emissions” said Alexander Boekhorst, VP Gas Processing and Conversion Technology at Shell. “We have continued to innovate and improve the value proposition of LNG using technology, and we look forward to collaborating with GE on this important initiative”.

GE's B&E class heavy-duty gas turbines can already operate today on 100% hydrogen emitting up to 25ppm NOx with the use of water in diffusion combustors. As part of this development agreement, GE is targeting gas turbine technology with the capability to operate on 100% hydrogen without the use of water while still maintaining NOx emissions.

The new DLN combustor technology is intended to become the backbone of new retrofittable system solutions for low-carbon operation of gas turbine while providing the reliability and availability required for LNG facilities. Dry operation also represents significant savings in water use and conservation: up 32,000 liters of water per hour are saved using DLN systems versus comparable alternatives.

DLN combustors are more efficient and do not use water as a diluent, thus offering LNG operators the ability to lower carbon and conserve water in their operations. In future, the developments to the DLN combustion technology could be installed on either new or existing 6B or 7E gas turbines. This would help reduce carbon emissions in industrial applications and LNG operations, particularly where water usage is challenging.

From desert climates to the tropics to the arctic cold, the B and E Class heavy-duty gas turbines provide essential power and perform in a vast number of duty cycles and applications in extreme climate conditions where reliability is key. These turbines can use more than 50 types of fuel— almost the entire fuel spectrum, including hydrogen —and can even switch fuels while running under full load.

 

About Shell plc

Shell plc is incorporated in England and Wales‚ has its headquarters in London and is listed on the London‚ Amsterdam‚ and New York stock exchanges. Shell companies have operations in more than 70 countries and territories with businesses including oil and gas exploration and production; production and marketing of liquefied natural gas and gas to liquids; manufacturing‚ marketing and shipping of oil products and chemicals and renewable energy projects.

For further information‚ visit www.shell.com. The companies in which Shell plc directly and indirectly owns investments are separate legal entities. In this document “Shell” is sometimes used for convenience where references are made to Shell plc and its subsidiaries in general.

 

About GE Gas Power
GE Gas Power is a world leader in natural gas power technology, services, and solutions. Through relentless innovation and continuous collaboration with our customers, we are providing more advanced, cleaner and efficient power that people depend on today and building the energy technologies of the future. With the world’s largest installed base of gas turbines and more than 670 million operating hours across GE’s installed fleet, we offer advanced technology and a level of experience that’s unmatched in the industry to build, operate, and maintain leading gas power plants. For more information, visit the company's website at  www.gepower.com. Follow GE Power on Twitter @GE_Power and on LinkedIn at GE Power.

GE Gas Power is part of GE Vernova, a dynamic accelerator comprised of our Power, Renewable Energy, Digital and Energy Financial Services businesses, focused on supporting customers’ transformations during the global energy transition.

For more information, contact:
Laura Aresi Public Relations Leader GE Gas Power [email protected]

end

Press Resources
vernova image
LNG Vessel
Image credit: Wojciech WrzesienShutterstock
(IMAGE/JPEG | 1.14MB)
Press release action

Open as PDF

Share